1.20 USART Driver Synchronous - USART Echo

This example echoes the received characters over the console using the USART driver in Synchronous mode.

Description

This example uses the USART driver in Synchronous mode in Bare-Metal environment to communicate over the console. It receives and echoes back the characters entered by the user.

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/usart/sync/usart_echo/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mz_ef_sk_freertos.XMPLAB X project for PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mz_ef_sk_freertos.XPIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up PIC32MZ Embedded Connectivity With FPU (EF) Starter Kit

  • Connect the Debug USB port on the board to the computer using a mini USB cable
  • Connect the USB to UART port on the board to the computer using a mini USB cable

Running the Application

  1. Open the Terminal application (e.g., Tera Term) on the computer.
  2. Connect to the EDBG Virtual COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 bits
    • Parity: None
    • Stop: 1 bit
    • Flow Control: None
  3. Build and program the application using its IDE.
  4. Type a character and observe the output on the console as shown below:
  5. LED toggles each time the character is echoed.
Refer to the following table for LED name: