3.1.1 Fuses - Factory Default Values

A clarification has been made for the Fuse Description section in regards to the fuse default values. The data sheet refers to these values as reset values when they should have been given as factory-programmed values. Also, they are given in both hexadecimal and binary values, which are contradicting each other.

The following sentence has been added to each sub-section of the Fuse Description section.

The default value given in this fuse description is the factory-programmed value, and should not be mistaken for the Reset value.

The table below lists the reset values given by the data sheet and the actual factory-programmed default values.

FuseStated Reset Value in Data SheetActual Factory Default on Device
HexadecimalBinaryHexadecimalBinary
WDTCFG-`b000000000x00`b00000000
BODCFG-`b000000000x00`b00000000
OSCCFG-`b0XXXXX010x01`b00000001
SYSCFG00xCF`b11XX01X00xF6`b11110110
SYSCFG1-`bXXXXX1110x07`b00000111
APPEND-`b000000000x00`b00000000
BOOTEND-`b000000000x00`b00000000
LOCKBIT-`b000000000xC5`b11000101