1.3.3.13 PAL_TxConfirm Typedef

C

typedef void (*PAL_TxConfirm)(PAL_RESULT result);

Summary

Pointer to a PAL Transmission Confirm event handler function.

Description

This data type defines the required function signature for the PAL transmission confirm event handling callback function. When PAL_Init is called, a client must register a pointer whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive transfer related event calls back from the PAL.

Parameters

ParamDescription
resultTransmission result reported as PAL_RESULT Enum

Returns

None.

Example

    static void _plcTxConfirm(PAL_RESULT result)
    {
        switch(result)
        {
            case PAL_RESULT_SUCCESS:
                break;
            case PAL_RESULT_ERROR:
                break;
            case PAL_RESULT_TIMEOUT:
                break;
        }
    }

    PAL_INIT palInitData;

    palInitData.palHandlers.palDataIndication = _plcDataIndication;
    palInitData.palHandlers.palTxConfirm = _plcTxConfirm;
    palInitData.palHandlers.palRxParamsIndication = _plcRxParamsIndication;

    PAL_Init(&palInitData);

Remarks

If the result is PAL_RESULT_SUCCESS, it means that the data was transferred successfully. Otherwise, result indicates the error type.