| PD-9001-10GS/AC does not power-up. | - Verify that a reliable power cord is used.
- Verify that the voltage at the power inlet is between 100–240 VAC.
- Remove and reapply power to the device and check the indicators during the power-up sequence.
|
| The PD does not operate. | - Verify that the PD is designed for PoE operation
according to IEEE® 802.3at standard.
- Verify that the cable used is a standard
straight‑wired cable, with four pairs (UTP/FTP Category 6a).
- Verify that the PD is connected to the PD-9001-10GS/AC Terminal port.
- If an external power splitter is in use, replace it with a known-good splitter.
- Remove and reapply power to the Midspan.
|
| The end device operates, but there is no data link. | - Verify that the cable used is a standard
straight-wired cable, with four-pair cable (UTP/FTP Category 5/5e/6).
- Verify that the Ethernet cable length is less than 100 meters from the Ethernet source to the load/remote terminal.
- Ensure that the input Ethernet cable is connected to the power injector’s
Ethernet port.
- If an external power splitter is
in use, replace it with a known-good splitter.
|