6.6 Sniffing Advertisement Packets Involving a Privacy Enabled Peripheral
The following are the steps to monitor advertisement packets, scan requests and scan responses to and from a single privacy-enabled device using the Bluetooth Low Energy Sniffer:
- Run the Bluetooth Low Energy Sniffer (if not already running).
- Input the IRK for the device. In Wireshark, choose IRK as the input key and enter the IRK in big-endian, hexadecimal format with a leading 0x in the input field.
- From the device list, select the device or choose “Follow IRK”.
Note: If the Bluetooth Low Energy Sniffer has previously successfully sniffed the pairing procedure, it remembers the IRK needed to identify the device. If not, the user needs to provide the IRK.