7 Plotting Power Consumption
The following instructions show how to analyze power consumption using the Power Debugger and Data Visualizer.
Note:
- For detailed information on the Power Debugger, refer to the Power Debugger User’s Guide
- For detailed information on the Data Visualizer, refer to the Data Visualizer User’s Guide
Power Debugger connection:
- Connect one of the ground reference pins of the Power Debugger to a ground pin on the Curiosity Nano board.
- Connect the VOFF pin on the Curiosity Nano board to a ground pin to turn off the connection between the USB power supply and the tinyAVR device.
- Connect the VBUS pin on the Curiosity Nano board to the input current pin of measurement circuit A on the Power Debugger.
- Connect the output current pin of measurement circuit A on the Power Debugger to the VTG pin on the Curiosity Nano board.
Data Visualizer setup:
- Open Data Visualizer.
- Open in Data Visualizer.
- On the DGI Control Panel pane, select .
- Check the Power check box.
- Expand the Channel A dropdown in the Control Panel in the Power Analysis pane.
- Drag the plug from A Current in the DGI Control Panel pane to the Current socket in the Power Analysis pane.
- Press in the DGI Control Panel pane.
- Optional: Enable cursors by checking the Enabled check box in the Cursors dropdown.