3.1.4.11 ICM_GetRegionDescriptor Function

C

ICM_REGION_DESCRIPTOR * ICM_GetRegionDescriptor(ICM_REGION_ID regionId);

Summary

Gets the pointer to the memory region descriptor.

Description

Gets the pointer to the memory region descriptor identifies with regionId parameter.

Precondition

None.

Parameters

ParametersDescription
regionIdIdentifies the memory region of ICM

Returns

Pointer to the descriptor data structure of the specified memory region.

Example

ICM_REGION_DESCRIPTOR *pRegionDescriptor;
ICM_SECONDARY_LIST icmSecList;

pRegionDescriptor = ICM_GetRegionDescriptor (ICM_REGION_0);
pRegionDescriptor->secondaryList = &icmSecList;
icmSecList.startAddress = (uint32_t)appMessageSHA1Sec;
icmSecList.transferSize = ICM_GetTransferSize(sizeof(appMessageSHA1Sec));
icmSecList.nextAddress = 0;

Remarks

None.