2.1.3.8 CRC32_Validate()
static bl_result_t CRC32_Validate (uint32_t startAddress, uint32_t length, uint32_t crcAddress)[static]
Validates the CRC32 checksum for a specified memory region.
This function checks the CRC32 checksum of a memory block against a stored CRC value to verify data integrity and then returns a value indicating whether the validation was successful or not.
| in | startAddress |
- The starting address of the memory block to validate |
| in | length |
- The length of the memory block in bytes |
| in | crcAddress |
- The address where the expected CRC32 checksum is stored |
BL_PASS - Bootloader verified the application image with no errors BL_FAIL - Bootloader encountered an error and failed unexpectedly BL_ERROR_VERIFICATION_FAIL - Bootloader image verification failed |