9 Read Operations
Read operations are initiated the same way as write operations with
the exception that the Read/Write Select bit in the device address byte must be a logic
‘1’. There are multiple read operations supported by the device:
- Current Address Read
- Random Address Read
- Sequential Read
The AT24CSW01x/AT24CSW02x contains a single Address Pointer register, which is shared by both the EEPROM and the Security register. As such, when changing from one region to the other, the first read operation in the new region should begin with a dummy write sequence (i.e. a random read operation with the new region’s device address and word address bytes) in order to ensure the Address Pointer is set to a known value. See Read Operations in the Security Register for additional requirements on read operations in the Security register.