8.4 Reading the Write Protection Register
To read the contents of the WPR, a random read operation must be sent to the device (see Random Read) so that the reserved word address bits A7 and A6 can properly be set. It is not possible to read the contents of the WPR with a current address read.
When reading the WPR contents, data bit 7 through 4 will always read as a
logic ‘0’ as seen in Table 8-4.
Note: # indicates the hardware address value
which is managed by the ordering code of the device (see Table 6-2).