10.2 MPLAB PICkit 5 In-Circuit Debugger

The debugger consists of an internal main board and an external USB Type-C connector and an 8-pin SIL connector. On the front of the debugger enclosure is an indicator light strip and a hidden push button located underneath the logo.
Figure 10-1. MPLAB® PICkit™ 5 In-Circuit Debugger
  1. Lanyard Connection - An opening through the top and side for a lanyard (not included) to be attached.
  2. Emergency Recovery Button - If needed, this recessed button is used for Recovery Boot Mode.
  3. USB Type-C Connector - Used to connect the debugger to the computer with the supplied USB cable.
  4. Indicator Light Strip - Displays the operational modes of the debugger (see Indicator Lights Strip).
  5. Button Area - The area in the center of the shield logo is used for the Programmer-To-Go1 option and for invoking the bootload mode (see How to Invoke the Bootload Mode).
  6. Pin 1 Marker - This designates the pin 1 location for proper connector alignment.
  7. Programming Connector - The connector is an 8-pin SIL connector (0.100" spacing) that connects to the target device (see Target Connection Pinouts).
  8. MicroSDHC Card Slot - The microSDHC card slot supports a large variety of microSDHC cards with various speed requirements.