Additional flexibility has been built into the Slot Access Policies of
the
ATECC608B-TFLXTLS device over that of the
ATECC608A-TNGTLS. This flexibility occurs in two areas:
- Whether slots are permanently
locked or slot lockable.
- Whether Secure Boot is
connected to a key and the Persistent Latch.
Slot Locking Options
Slot locking options are called out for each individual slot and will be one of two
types.
- Slot Lockable
- A slot that has the slot lock option set allows for the end user to lock the
slot at some point in the future after the initial manufacturing phase. This
can be used to allow for a key to be set during a subsequent manufacturing
step outside of Microchip or by the end user. The slot can be locked using
the
Lock command. Once the slot has been locked, no future
modifications to the data in the slot is possible. - Permanent Lock
- A permanently locked slot is never able to be updated once it
leaves the Microchip manufacturing facilities. The correct data or key must
be provided to Microchip prior to the provisioning of these devices.
Secure Boot Option
The Secure Boot Access Policies provide an option to limit what commands are run
prior to a successful secure boot or to provide unlimited command access. The
Private Key in Slot 0 may be set to require a Secure Boot before this key will be
authorized for use for most commands. To use this feature, a change to the
SecureBoot Configuration Settings and to the Key Configuration values are required.
These configuration changes will set the Persistent Latch upon a successful Secure
Boot. The Slot Access Policy changes for Slot 0 tie usage of the key to the
Persistent Latch being set.
Persistent Latch Operation
The Persistent Latch will retain state even during Idle and Sleep modes. This allows
for a single Secure Boot operation to be run only once after initial power-up. If
the device supply voltage goes below the minimum allowed value, the Persistent Latch
will be reset and a new Secure Boot operation will need to be performed.
Prototype Units
Prototype units come with a specific
default configuration that cannot be changed. The default configuration have all
slots options set to Slot Lockable. This provides maximum flexibility when
developing software to reprogram keys by an application. The final configuration
does not need to be set this way. The Secure Boot option is not available with the
prototype units. This option can only be selected for production units. Prototype
units are also only available with an I2C interface.
Detailed Slot
Configurations
The following tables provide a more detailed description of the slot
configuration and key configuration settings for each configured slot on the device.
Relevant commands and command modes applicable to each configured slot are included.
The table provides all allowed Key and Slot
Configuration Values available for the ATECC608B-TFLXTLS device on a slot by slot basis. These options are
available for both I2C and SWI options.
Table 2-3. Slot 0 Configuration
Information| Slot | Configuration Value | Description of
Enabled Features |
|---|
| 0 | Option 1:
Persistent Latch is not connected to Slot |
| Key: | | Primary Private Key- Contains P256
NIST ECC private key
- The
corresponding public key can always be generated
- Random nonce
is required
|
| Slot: | |
- Slot is
secret
- Can sign
external messages
- Can use with
ECDH command
|
| Option 2: Slot is Connected to Persistent Latch |
| Key: | |
- Same as
Option 1
- Persistent
Disable Option Enabled
|
| Slot: | |
|
Table 2-4. Slot 1 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 1 | Key: | | Internal Sign Private Key - Contains P256
NIST ECC private key
- The
corresponding public key can always be generated
- Random nonce
is required
|
| Slot: | |
- Slot is
secret
- Can sign
internal messages generated by GenDig or GenKey
- ECDH
disabled
|
Table 2-5. Slot and Key Configuration
Slots 2-4| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 2,3 or 4 | Option 1: Slot Lockable |
| Key: | | Secondary Private Keys 1-3- Contains P256
NIST ECC private key
- The
corresponding public key can always be generated
- Random nonce
is required
- This slot can
be individually locked
|
| Slot: | |
- GenKey can be
used to generate a new ECC private key in this slot prior to
locking
- Slot is
secret
- Can sign
external messages
- Can use with
ECDH command
|
| Option 2: Permanent Key |
| Key: | |
- Same as
Option 1 except slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except GenKey can not be used
|
Table 2-6. Slot 5 Configuration
Information| Slot | Configuration
Value | Description of Enabled Features |
|---|
| 5 | Option #1 Slot
Lockable |
| Key: | | Secret Key- Slot can
store up to 2 AES 128-bit (16 byte) symmetric keys
- This slot can
be individually locked
|
| Slot: | |
- New symmetric
key can be written with an encrypted write only
- Key in slot 6
is the key used to encrypt the write
- The contents
of the slot are secret
- Slot cannot
be used for the
CheckMac Copy command
|
| Option #2
Permanent Key |
| Key: | |
- Same as
Option 1 except slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except an Encrypted Write can not be performed
|
Table 2-7. Slot 6 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 6 | Option #1:
Slot is Lockable |
| Key: | | IO Protection Key- Can contain a
SHA256 symmetric key or other data. If the IO protection key
is not used, this slot can be used for other data
- A random
nonce is required when this key is used
- This slot can
be individually locked
|
| Slot: | |
- Data can be
written in the Clear
- The contents
of this slot are secret and cannot be read
- Slot cannot
be used for the
CheckMac Copy command
|
| Option 2: Permanent Lock |
| Key: | |
- Same as
Option 1 except slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except the slot cannot be written/
|
CAUTION: In general, the I/O protection key stored in Slot 6
must be left to be Slot Lockable. In most cases the I/O Protection key is often
unique to each device. If for some use case the I/O Protection key is the same for
all devices then a Permanent Lock Option can be selected.
Table 2-8. Slot 7 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 7 | Key: | | Secure Boot Digest- This slot is
designated to be used for other data.
|
| Slot: | |
- This slot
cannot be directly written or read
- This slot is
secret and cannot be used by the
MAC
command - This slot
cannot be used for
CheckMac Copy
command
|
Table 2-9. Slot 8 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 8 | Option 1:
Slot Lockable |
| Key: | | General Data- This slot is
designated for use with general data
- Slot is
lockable
|
| Slot: | |
- Clear text
writes and reads are permitted to this slot
- Slot cannot
be used for the
CheckMac Copy command
|
| Option 2: Permanent Lock |
| Key: | |
- Same as
Option 1 except slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except the slot cannot be written/
|
Table 2-10. Slot 9 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 9 | Key: | | AES Key - Slot can
store up to four AES 128-bit symmetric keys
|
| Slot: | |
- Clear text
writes are allowed to this slot
- This slot is
secret
- Slot cannot
be used for the
CheckMac Copy command
|
Table 2-11. Slot 10 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 10 | Option 1:
Permanently Locked |
| Key: | | Device Compressed Certificate- Slot defined
to store other data
|
| Slot: | |
- Data cannot
be overwritten
- Data can be
read in the clear
|
|
Option 2: Slot Lockable Note: This Configuration is Used for Prototype Units
|
| Key: | |
- All features
as shown in Option 1
- Slot is
lockable
|
| Slot: | |
- Same as
Option 1 except the slot can be written
|
Table 2-12. Slot 11 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 11 | Option 1:
Permanently Locked |
| Key: | | Signer Public Key- Slot is
defined for ECC key
- ECC key is a
public key
|
| Slot: | |
- Data cannot
be overwritten
- Data can be
read in the clear
|
|
Option 2: Slot Lockable Note: This Configuration is Used for Prototype Units
|
| Key: | |
- All features
as shown in Option 1
- Slot is
lockable
|
| Slot: | |
- Same as
Option 1 except the slot can be written
|
Table 2-13. Slot 12 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 12 | Option 1:
Permanently Locked |
| Key: | | Signer Compressed Certificate- Slot defined
to store other data
|
| Slot: | |
- Data cannot
be overwritten
- Data can be
read in the clear
|
|
Option 2: Slot Lockable Note: This Configuration is Used for Prototype Units
|
| Key: | |
- All features
as shown in Option 1
- Slot is
lockable
|
| Slot: | |
- Same as
Optoin 1 except the slot can be written
|
Table 2-14. Slot 13 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 13 | Option 1:
Slot Lockable |
| Key: | | Parent Public Key or General Data- Slot is
defined for ECC key
- Slot is
lockable
|
| Slot: | |
- Slot can be
written in the clear (unless locked)
- Slot can
always be read
|
| Option 2: Permanently Locked |
| Key: | |
- Same as
Option 1 except the slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except the slot cannot be written
|
Important: If Slot 13 is configured as a Parent Public Key, in
general it must be set to a Permanent Key and must not be updatable. For general
data, either option can be selected.
Table 2-15. Slot 14 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 14 | Key: | | Validated Public Key- Slot is
defined for ECC key
- Public key
can be used by the
Verify command if the
key has been validated
|
| Slot: | |
- Write mode
set to PubInvalid
- Can write to
slot if key is invalidated first
- Slot can
always be read in the clear
|
Table 2-16. Slot 15 Configuration
Information| Slot | Configuration Value | Description of Enabled
Features |
|---|
| 15 | Option 1:
Slot is Lockable |
| Key: | | Secure Boot Public Key- Slot is
defined for ECC key
- Slot is
lockable
|
| Slot: | |
- Always
writable unless locked
- Slot can
always be read
|
| Option 2: Permanently Locked |
| Key: | |
- Same as
Option 1 except the slot is permanently locked
|
| Slot: | |
- Same as
Option 1 except the slot cannot be written
|