5.1.3 Lock Command
For the ATECC608B-TFLXTLS, the
Configuration zone has already been locked and the access
policies of the Data zone have already been set. However,
several of the data slots can still be updated through the
use of other commands. If so desired, some of these slots
can be permanently locked from future updates by using the
Slot Locking mode of the Lock
command.