5 Hardware Development
If the user decides to develop their own hardware, refer to the guidelines from the ATA8510/15 Industrial User's Guide and ATA8510/ATA8515 UHF ASK/FSK Transceiver Data Sheet. The instructions from the application section in the ATA8510/15 Industrial User's Guide must be followed to ensure the specified performance. For further details about the hardware documentation, refer to the tool package available in the latest version of the ATA8510 EK1 Tool Pack.
The Microchip hardware is developed according to all recommendations and guidelines from the technical documentation. The user can reuse these hardware resources for developing their own application. If the user requires a unique application that is not covered by documentation or hardware examples, request further support from www.microchip.com/support.