1.4 TCP/IP TCP Client Server
This demonstration is a combination of the TCP Client and TCP Server application.
It shows the usage of MPLAB Harmony TCP API to implement,
- a TCP echo server on port 9760.
- a TCP client that establishes TCP/IP connection to a TCP server.
Description
The TCP/IP TCP Client Server application is based on MPLAB® Harmony 3 TCP/IP Stack.
The Harmony TCP/IP stack is a collection of different network protocols.
The source files of Harmony 3 TCP/IP stack is available here.
The demo is created with MPLAB X IDE and MCC plugin.
MCC Project Graph - TCP/IP TCP Client Server
The following Project Graph shows the Harmony components included in the TCP/IP TCP Client Server demo application.

TCP/IP Configuration - TCP/IP TCP Client Server
The TCP/IP modules enabled for the demo is shown in the TCP/IP Configuration Overview
More details of TCP/IP Configuration plugin is available here

The Ethernet interface in the above configuration use 1 Gbps internal GMAC peripheral and Gigabit Ethernet PHY Transceiver KSZ9131.
The Application Layer modules enabled in the demo are as follows:
- Application Layer
Modules
- DHCP Client to discover the IPv4 address from the nearest DHCP Server.
- DNS Client provides DNS resolution capabilities to the stack.
The Ethernet interface in this demo use internal GMAC peripheral and Gigabit Ethernet PHY Transceiver KSZ9131.
Downloading and Building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps\tcpip_tcp_client_server\firmware .
To build the application, refer to the following list of demo configurations and open the project using MPLAB X IDE.
| Project Name | Target Device | Development Board | Description |
|---|---|---|---|
| sam_a7g5_ek_GMAC0.X | SAMA7G54 | SAMA7G54-EK | TCP/IP TCP Client Server with Gigabit Ethernet - Bare Metal |
| sam_a7g5_ek_GMAC0_freertos.X | SAMA7G54 | SAMA7G54-EK | TCP/IP TCP Client Server with Gigabit Ethernet - FreeRTOS |
Hardware Setup
The target board for running the application is SAMA7G54-EK.
This section provides essential hardware configuration of this target board to run TCP/IP applications.

Board Setup
To set up the hardware, refer to the section Board Setup in SAMA7G54-EK User Guide.
- For Gigabit Ethernet connection, connect Ethernet cable between RJ45 socket (J5) and router/switch/computer.
- For 10/100 Ethernet connection, connect Ethernet cable between RJ45 socket (J6) and router/switch/computer.
Setting up at91bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader.
Refer to the at91bootstrap loader documentation for details on how to configure and run/debug the application using MPLABX and booting application using an SD Card.
Running the Application
- Open a terminal application on the host computer (like Hyper-terminal or Tera Term).
- Configure the terminal application for serial port connected to JLink CDC UART Port.
- Set baud rate as 115200 in the terminal application.
- Build and download the application project on the target board.
- For 1000 Mbps operation, ensure connection from Gigabit(1000Mbps) capable network socket of a router/switch/computer to socket J5 on the board. For 10/100 Mbps operation, connect to socket J6.
- Verify the TCP/IP Stack initialization console messages.
GMAC0 - Console Start up

If DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board.
This will be printed on the console. Otherwise, the default static IP address will be assigned to the board.
TCP Client Test
Enter following command in console: openurl <url>. For example, openurl http://www.microchip.com/.
The response from the server will be printed on the console as shown below.

TCP Server Test
For TCP Server test, a TCP Client application is required to run on the host computer (SocketTest, PacketSender etc).
In this demonstration, we use PacketSender utility.
- Send a TCP packet to the IP
address of the hardware board, port 9760, from TCP Client application
(PacketSender) running on the computer. See the following
screenshot.

- The TCP Server running on the
hardware board will echo back the message it receives. See the console
screenshot.