1.2.8 SAM E54 Xplained Pro Evaluation Kit: Building and Running the USB Host MSD Bootloader Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can be download using content manager by following these instructions.

Path of the application within the repository is apps/usb_host_msd_bootloader/.

To build the application, refer to the following table and open the project using its IDE.

Setting Up SAM E54 Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable
  • Use TARGET USB connector on the board to connect the USB device to the USB Host
    • A USB micro AB to type A USB Host receptacle converter will be needed to connect the type A USB Flash Drive to the device

Running the Application

  1. Open the test application project test_app/firmware/sam_e54_xpro.X in the IDE.
  2. Build the project to generate the binary (Do not program the binary).
  3. Open the bootloader project bootloader/firmware/sam_e54_xpro.X in the IDE.
  4. Build and program the application using the IDE.
  5. LED0 will be turned-on once programming is completed and bootloader starts running.
  6. Open the Terminal application (e.g., Tera Term) on the computer to get test application messages through UART once bootloaded.
  7. Configure the serial port settings as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  8. Copy the generated application binary file to a USB Flash drive from the Host PC.
    • <harmony3_path>\bootloader_apps_usb\apps\usb_host_msd_bootloader\test_app\firmware\sam_e54_xpro.X\dist\sam_e54_xpro\production\sam_e54_xpro.X.production.bin
  9. Rename the copied application binary file to image.bin.
  10. Insert the USB Flash Drive with the application binary image.bin to the Host connector on the device.
  11. Once the application is successfully programmed LED0 should start blinking and the user should see below output on the console.
  12. Remove the USB Flash Drive from the Host connector.
  13. Press and hold the Switch SW0 to trigger Bootloader from test application and the user should see below output.
  14. Repeat Steps 10-12 once and jump to Step 15.
    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 13
  15. Press and hold the Switch SW0 and then press Reset button or Power cycle the device to force trigger bootloader at startup.
  16. Repeat Steps 10-12 once.
    • This step is to verify whether bootloader is triggered by switch press at reset