11.3 Locating Functions at a Specific Address
In this example, the C language function
func is located at a specific
address.#include <stdio.h>
void __attribute__((address(0x9d002000))) func(void)
{ ... }The equivalent function definition in assembly language appears below. The
.align directive is optional and represents the
default alignment in program memory. Use of * as a
section name causes the assembler to generate a unique name based on the source file
name..section *,address(0x9d002000),code
.align 2
.globl func
func:
......