5.8.3 Irpc Directive
The .irpc symbol,
value
...
.endr directive evaluate a sequence
of statements assigning different values to symbol. The
sequence of statements starts at the .irpc directive, and
is terminated by an .endr directive. For each character
in value, symbol is set
to the character, and the sequence of statements is assembled. If no value is listed, the
sequence of statements is assembled once, with symbol set to the null string. To refer to
symbol within the sequence of statements, use \symbol.
For example, assembling:
.irpc reg,0123
lw $a\reg, 1032+\reg($sp)
.endris equivalent to
assembling:lw $a0,1032+0($sp)
lw $a1,1032+1($sp)
lw $a2,1032+2($sp)
lw $a3,1032+3($sp)