5.5.1 Align Directive
The .align [algn[,
fill]] directive pads the location counter (in the current
subsection) to a particular storage boundary. The first expression (which must be absolute)
is the alignment required specified as the number of low-order zero bits the location
counter must have after advancement.
The assembler accepts algn values from 0
up to 15. A .align 0 turns off the automatic alignment
used by the data creating pseudo-ops. You must make sure that data is properly aligned.
Reinstate auto alignment with a .align directive.
The second expression (also absolute) gives the
fill value to be stored in the padding bytes. It
(and the comma) may be omitted. If it is omitted, the padding bytes are zero. You may wish
to use a fill value of 0xFF for regions of Flash memory.