5.3.4 Lcomm Directive
The .lcomm symbol,
length directive reserves
length bytes for a local common denoted by
symbol. The section and value of symbol are those
of the new local common. The addresses are allocated in the .bss section, so that at run-time, the bytes start off zeroed.
symbol is not declared global so it is normally not
visible to the linker.