10.2.3.1 Allocation of Code-attributed Sections
The code section attribute specifies that a section
should be allocated in program memory, as defined by region
kseg0_program_mem in the linker script for PIC32M devices. The
following attributes may be used in conjunction with code and will further
specify the allocation:
address()specifies an absolute address.alignspecifies alignment of the section starting address