10.2.3.3 Allocation of Bss-attributed Sections
The bss section attribute specifies that a section should
be allocated as uninitialized storage in data memory, as defined by region
kseg0_data_mem and kseg1_data_mem in the linker script
for PIC32M devices. The following attributes may be used in conjunction with
bss and will further specify the allocation:
address()specifies an absolute address.alignspecifies alignment of the section starting address