10.2.3.2 Allocation of Data-attributed Sections
The data section attribute specifies that a section
should be allocated as initialized storage in data memory, as defined by regions
kseg0_data_mem and kseg1_data_mem in the linker script
for PIC32M devices. The following attributes may be used in conjunction with data and will
further specify the allocation:
address()specifies an absolute address.alignspecifies alignment of the section starting address