3.3.1.1 Omit False Conditionals Listing Option
The
-ac form of this option omits false
conditionals from a listing. Any lines that are not assembled because of a false .if or .ifdef (or the
.else of a true .if
or .ifdef) will be omitted from the listing. The
following example shows a listing where the -ac option
was not used.GAS LISTING asm.s page 1
1 # 1 "asm.S"
2 # 1 "<built-in>"
1 .data
0
2 .if 0
3 .if 1
4 .endif
5 .long 0
6 .if 0
7 .long 0
8 .endif
9 .else
10 .if 1
11 .endif
12 0000 02000000 .long 2
13 .if 0
14 .long 3
15 .else
16 0004 04000000 .long 4
17 .endif
18 .endif
19 .if 0
20 .long 5
21 .elseif 1
22 .if 0
23 .long 6
24 .elseif 1
25 0008 07000000 .long 7
26 .endif
27 .elseif 1
28 .long 8
29 .else
30 .long 9
31 .endifThe next example shows a listing for the same source where the
-ac option
was used.GAS LISTING asm.s page 1
1 # 1 "asm.S"
2 # 1 "<built-in>"
1 .data
0
0
2 .if 0
9 .else
10 .if 1
11 .endif
12 0000 02000000 .long 2
13 .if 0
15 .else
16 0004 04000000 .long 4
17 .endif
18 .endif
19 .if 0
21 .elseif 1
22 .if 0
24 .elseif 1
25 0008 07000000 .long 7
26 .endif
27 .elseif 1
29 .else
31 .endifNote: Some lines omitted due to
-ac option.