22.2.1 Capture Sources

In Capture mode, the CCPx pin may be configured as an input by setting the associated TRIS control bit.

Important: If the CCPx pin is configured as an output, a write to the port can cause a Capture condition.

The capture source is selected by configuring the CTS bits as shown in the following table:

Table 22-2. Capture Trigger Sources
CTSSource
111CLC4_out
110CLC3_out
101CLC2_out
100CLC1_out
011IOC_interrupt
010C2_out
001C1_out
000Pin selected by CCPxPPS