3 Transient Response With ACOT Control
One of the biggest advantages of ACOT control is its superior load transient response compared to fixed frequency control (Current mode control or Voltage mode control). The following sections provide a closer look at the step-up and step-down load transient behaviors of each control mode.
Step-up Load Transient
As illustrated in Figure 1, ACOT applies only a minimum OFF time during load step-up transients, ensuring the high side power switch is turned on for a sufficient duration to accommodate the rapid increase in load without compromising stability. This also means ACOT increases the switching frequency during step-up load transients, enabling swift response to sudden load changes and maintaining optimal performance.
Importantly, ACOT maintains a consistent pulse width during load transients, ensuring stable regulation without significant output voltage fluctuations. This could be explained by the response delay in ACOT, which is reduced to the minimum OFF time, ensuring rapid and precise adjustments to load variations for enhanced voltage regulation and system stability.
Figure 1 also includes the behavior of fixed frequency control during step-up load transient for comparison. Unlike ACOT, fixed frequency control maintains a constant switching frequency during step-up load transient, which may limit its ability to promptly respond to sudden load variations, affecting transient performance. The delay associated with such control methods can be significant, as severe in the extreme as approaching the clock period (Tclock), compromising response time in dynamic operating conditions.
Step-down Load Transient
ACOT controllers dynamically reduce the switching frequency in response to a step-down load transient, effectively managing the overshoot in output voltage caused by the sudden reduction in load current. This approach leverages ACOT's faster loop response, resulting in minimal delay for output voltage correction. As shown in Figure 2, if the ACOT controller can operate at 0% duty cycle, it may skip switching cycles altogether to prevent excessive voltage overshoot. This capability allows ACOT controllers to react quickly and efficiently to load changes, maintaining output voltage stability.
In contrast, even though fixed-frequency controllers reduce the duty cycle during step-down transient, they still maintain a constant switching frequency which results in a longer correction time compared to ACOT. However, many modern controllers come with 0% duty cycle capability, allowing them to skip cycles during an output voltage overshoot and perform similarly to ACOT controllers during step-down load transients.
Numerous factors influence the transient response in a buck converter, including the design and performance of the control loop, switching frequency, output LC filter design, type of output capacitor, load step size, slew rate, and more. Given the focus on ACOT control, how ripple injection design can influence load transient performance will be examined in AN7166 - ACOT Design Guide: Control-Loop Analysis and Performance Optimization.