3.3.1.1 flags Struct
This is the flags structure that is used in the SW_CLOCK_PERIODIC_MONITOR_02. It contains the two flags in the test which are updated and checked while performing the SW_CLOCK_PERIODIC_MONITOR_02.
Members
- unsigned pulseFound
- This is set in the Timer1 Gate ISR function when a pulse is detected
- unsigned testStatus
- This flag controls if the test is still in progress or if it has completed.