4.1.2 PIC32CM LS00 Curiosity Nano+ Touch Base Quick Reference
The following figure shows a simplified reference to enable quicker development with the Curiosity Nano+ Touch Base for Click boards, AC164162. For additional information, visit https://www.microchip.com/en-us/development-tool/ac164162.
Note: As a result of dedicated lines being assigned for the touch
button and the device USB, some pin assignments that go out to the 48 pin edge connector
(J5) are impacted in the following way:
- No microcontroller pin is assigned for the PWM3 line (J5 pin 40). As a result, as shown in Figure 4-2, the 3rd mikroBUS connector and the EXT1 connector of the Curiosity Nano Base for Click board do not have a PWM connection.
- The PA07 pin of the microcontroller is shared between RST2 (J5 pin 19) and RST3(J5 pin 31). As a result, the RST lines of the 2nd and 3rd mikroBUS connectors and the EXT1 connector of the Curiosity Nano Base for Click board are shared.
Users need to ensure these adjustments are considered while developing their applications.