4.1.1 PIC32CM LS00 Curiosity Nano+ Touch Pinout
Excluding the USB peripheral control pins, PA24 and PA25, most of the PIC32CM5164LS00048 I/O pins are accessible through the edge connectors on the PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit. The following figure shows the evaluation kit pin out.
Note: The PA30 and PA31 pins are only available at the edge connector
in the debugger section if the cut straps on the bottom have continuity.