3.5.1 Getting Started Application on PIC32CM JH VL Curiosity Nano+ Touch Evaluation Kit
Description
This application demonstrates an LED toggle on timeout basis and print the LED toggling rate on the serial terminal. The periodicity of the timeout will change from 500 milliseconds to 1 second, 2 seconds, 4 seconds and back to 500 milliseconds each time the switch on the PIC32CM JH VL Curiosity Nano+ Touch evaluation kit is pressed.
Modules/Technology Used
- Peripheral Modules
- EIC
- RTC
- GPIO
- DMAC
- SERCOM (USART)
The following figure provides the MCC Harmony project graph with all the components.
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
Refer to the Project Manifest present in
harmony-manifest-success.yml under the project folder
firmware/src/config/pic32cm_jh_vl_cnano.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
- Any Serial Terminal application, such as Tera Term/PuTTY terminal application
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected, it is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Connect the PIC32CM JH VL
Curiosity Nano+ Touch evaluation kit to the Host PC as a USB device
through a Type-A male to Type-C USB cable connected to Type-C USB (Debug
USB) port
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to
File>Import>Hex/ELF File - In the Import Image File
window,
- Create Prebuilt
Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CM6408JH00064
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project
Name and Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt
Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section
Programming/Debugging Application Project
- Open the project
(
pic32cm_jh_vl_cnano_getting_started/firmware/pic32cm_jh_vl_cnano.X) in MPLAB X IDE - Ensure
PIC32CM JH VL Curiosity Nanois selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section
Running the Demo
- Open the Tera Term/PuTTY terminal application on the PC (from the Windows® Start menu by pressing the Start button)
- Set the baud rate to 115200
- An LED on the PIC32CM JH VL Curiosity Nano+ Touch evaluation kit toggles on every timeout basis and the default periodicity of the timeout is 500 milliseconds
- And, the LED toggling rate is displayed on the serial terminal
- Press the switch on the PIC32CM JH VL Curiosity Nano+ Touch evaluation kit to change the default periodicity of the timeout to 1 second
- Every subsequent pressing
of the switch SW200 on the PIC32CM JH VL Curiosity Nano+ Touch
evaluation kit changes the periodicity of the timeout to 2 seconds, 4
seconds, 500 milliseconds, and back to 1 second in cyclic order
- The console displays the
following message
Comments
- Reference Training Module: Getting Started With MPLAB® Harmony v3 Peripheral Libraries on PIC32CM JH (Arm® Cortex®-M0+) MCUs
- This application demo
builds and works out of box by following the instructions in Running the
Demo section. If the user needs to enhance/customize this application
demo, should use the MPLAB Harmony v3 Software framework. Refer to the
following links to setup and build the applications using MPLAB
Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project