9.2.3.2 Multiple Value Parameters
These parameters may have more than one value.
When reading all values, the parameter ID can be used, however when accessing a single value
within the set of all values the command will use a fractional
integer form of the ID consisting of
<ID>.<INDEX>
>AT+CMD=5
+CMD:5.0,"value1"
+CMD:5.1,"value2"
+CMD:5.2,"value3"
OK>AT+CMD=5.1
+CMD:5.1,"value2"
OKWhen writing a value, the behaviour will depend on the implementation of the command, however
often writing a value to the parameter
<ID> will cause an additional
value to be appended to the set of parameter values, writing to
the fractional <ID>.<INDEX> will
cause that parameter index to be updated.
>AT+CMD=5
+CMD:5.0,"value1"
OK
>AT+CMD=5,"newvalue"
OK
>AT+CMD=5
+CMD:5.0,"value1"
+CMD:5.1,"newvalue">AT+CMD=5
+CMD:5.0,"value1"
+CMD:5.1,"value2"
OK
>AT+CMD=5.0,"newvalue"
OK
>AT+CMD=5
+CMD:5.0,"newvalue"
+CMD:5.1,"value2"