Mount the AVR128DB48 Curiosity Nano host board, the Serial
Flash board and the RNWF02 Add On Board on
Curiosity Nano base board at respective headers as illustrated in the following
figure.Figure 6-23. Host Board Setup for
OTA Demo
Connect the debugger USB port on
the AVR128DB48 Curiosity Nano board to computer
using a micro USB cable
Open the project and launch MCC
with Melody Content Manager Tool
Configure Home-AP credentials for STA mode, using the Wi-Fi settings
configuration. For more details about the Wi-Fi settings configuration, See
Figure 3-14
Generate the code as illustrated
below Figure 6-24. Generating the
Code
Build and program the code to the
hardware using MPLAB X IDEFigure 6-25. Programming the
Board
Open the Terminal application
(for example, Tera Term or PuTTY) on the PC
Connect to the host board COM
port and configure the serial settings as follows:
Baud: 115200
Data: 8 Bits
Parity: None
Stop: 1 Bit
Flow Control:
None
Press the SW0 (Soft Reset) button on the host board, see Figure 6-1.
The board boots up and connect to
Home-AP, as per the configurations given in Step 4. After the successful Wi-Fi connection the device opens up a TCP tunnel and
wait for the OTA server and firmware image details from the configurator
tool.Figure 6-26. Initial Firmware
Version, OTA Enable
Three example sample firmware
binaries are available in the ./ota_demo/tools folder.
From File explorer,
navigate to the folder (./ota_demo/tools)Figure 6-27. Tools
Folder
In the address bar, type
cmd and hit enterFigure 6-28. CMD
This will open up a
terminal window, located in this folderFigure 6-29. Terminal
Window
Start an HTTP server,
enter python -m http.server. By default it will be
listening on port 8000Figure 6-30. python -m
http.server
Run the python OTA configurator
tool from the ./ota_demo/tools folder, as illustrated in the
following figure
From File explorer, navigate to the folder
(./ota_demo/tools)Figure 6-31. Tools Folder
In the address bar, type cmd and hit enterFigure 6-32. CMD
This will open up a terminal window, located in this folderFigure 6-33. Terminal Window
Run the python OTA
configurator by typing python mchp_configurator.py.
Follow the instructions on the terminal, enter HTTP server IP, port and
Image file name to be downloaded by RNWF.
Note: Hit Enter when
requested to enter IP and port and it will default to the computer
IP and port 8000
Figure 6-34. OTA
Configurator
Now the device creates a HTTP link with the OTA server and starts downloading
the image file.Figure 6-35. Image Download
After successfully downloading
the image, the DFU is triggered and firmware is Flashed into the RNWF02 moduleFigure 6-36. DFU Progress
Upon successful DFU, the host
will Reset and print the RNWF02 module’s new
firmware informationFigure 6-37. Updated
Firmware
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.