3.1.7.7.2 MQTT System Service Interface
This section describes the MQTT System Service Interface
MQTT Service Status Enum
States involved in the operation of the MQTT state
machine.
typedef enum
{
RNWF_MQTT_CONFIG, /**<Configure the MQTT Broker parameters*/
RNWF_MQTT_CONNECT, /**<Connect to the MQTT Broker */
RNWF_MQTT_RECONNECT, /**<Request reconnect to the MQTT Cloud*/
RNWF_MQTT_DISCONNECT, /**<Trigger Disconnect from MQTT Broker*/
RNWF_MQTT_SUBSCRIBE_QOS0, /**<Subscribe to QoS0 Topics */
RNWF_MQTT_SUBSCRIBE_QOS1, /**<Subscribe to QoS1 Topics */
RNWF_MQTT_SUBSCRIBE_QOS2, /**<Subscribe to QoS2 Topics */
RNWF_MQTT_PUBLISH, /**<Publis to MQTT Broker*/
RNWF_MQTT_SET_CALLBACK, /**<Configure the MQTT Application Callback*/
}RNWF_MQTT_SERVICE_t;MQTT Event Enum
Events involved in the operation of the MQTT state
machine
typedef enum
{
RNWF_MQTT_CONNECTED, /**<Connected to MQTT broker event */
RNWF_MQTT_DISCONNECTED, /**<Disconnected from MQTT broker event*/
RNWF_MQTT_SUBCRIBE_MSG, /**<Event to report received MQTT message*/
}RNWF_MQTT_EVENT_t;MQTT Message Configuration Struct
Defines the configuration parameters required to establish connection
with MQTT
Broker
typedef struct
{
const char *url; /**<MQTT Broker/Server URL */
uint16_t port; /**<MQTT Broker/Server Port */
const char *clientid;
const char *username; /**<MQTT User Name Credential */
const char *password; /**<MQTT Password Credential */
uint8_t tls_idx;
uint8_t *tls_conf;
}RNWF_MQTT_CFG_t;MQTT Message Enum
typedef enum
{
NEW_MSG, /**New message*/
DUP_MSG /**Duplicate message*/
}RNWF_MQTT_MSG_t;
MQTT QoS Enum
typedef enum
{
MQTT_QOS0, /**<No-Ack, Best effort delivery(No Guarantee)*/
MQTT_QOS1, /**<Pub-Ack, sent untill PUBACK from broker(possible duplicates) */
MQTT_QOS2, /**<Highest service, no duplicate with guarantee */
}RNWF_MQTT_QOS_t;
MQTT Publish Retain Enum
Sets whether the published message is retained at the broker or
not.
typedef enum
{
NO_RETAIN, /**<Publish message is not saved at broker */
RETAIN, /**<Publish message is saved at broker */
}RNWF_MQTT_RETAIN_t;MQTT Frame Struct
typedef struct
{
RNWF_MQTT_MSG_t isNew; /**<Indicates message is new or duplicate */
RNWF_MQTT_QOS_t qos; /**<QoS type for the message ::RNWF_MQTT_QOS_t */
RNWF_MQTT_RETAIN_t isRetain; /**<Retain flag for the publish message */
const uint8_t *topic; /**<Publish topic for the message */
const uint8_t *message; /**<Indicates message is new or duplicate */
}RNWF_MQTT_FRAME_t;