1.1.1.6 Summary of State Machine Classes
| Class | Name | Next-State | Output |
|---|---|---|---|
| Class 0 | Combinatorial Logic | State does not exist | Output depends upon the inputs with no delay (combinatorial) |
| Class 1 | Delay | State depends upon the inputs alone to delay the output | Output is same as Class 0 but delayed by one state time |
| Class 2 | State output, direct state transition | Next-state depends upon the previous state, hence forming a sequence of states | Output depends upon the current state. Each state can produce only one output. |
| Class 3 | State output, conditional state transition (Moore) | Next-state depends upon both the previous state and the inputs, hence having the ability to have alternate state sequences | Output depends upon the current state. Each state can produce only one output. |
| Class 4 | Conditional state output, conditional state transition (Mealy) | Next-state depends upon both the previous state and the inputs, hence having the ability to have alternate state sequences | Output depends upon the current state and inputs. Each state may produce multiple outputs. |
Legend: Q = Inputs/Qualifiers to the state machine I = Outputs/Instructions from the state machine X = State of the machine (Represents “next-state” if followed by ) T = State time g = Next-state function f = Output function | |||