3.4 Test Software Application
The ATA8350_Test.zip software package includes ATA8350 test software to perform
the following tests:
- TX spectrum measurements
- BER measurements
- Crystal calibration
The test software includes two projects:
UWB_PC_Test4.cprojto be used with a PC terminal program and a USB PC connectionUWB_OLED_Test4.cprojto be used with the ATOLED1 extension board and a USB power supply
The following figure shows the test menu when using the test software with a PC terminal application with the following settings:
- 115200 baud rate
- 8 data bits
- 1 stop bit
- No parity
The following tests can be performed with this application (For more details about the test
setup, see the
ATA8350_Test.zip software package and [7].):- 0: TX_CHA F0+Fm TX test at the upper modulation frequency of the 6.52 GHz channel
- 1: TX_CHA F0-Fm TX test at the lower modulation frequency of the 6.52 GHz channel
- 2: TX_CHA F0+/-Fm TX test at both modulation frequencies of the 6.52 GHz channel
- 3: TX_CHB F0+/-Fm TX test at both modulation frequencies of the 7.04 GHz channel
- 4: TX_CHC F0+/-Fm TX test at both modulation frequencies of the 7.56 GHz channel
- 5: TX_CHA PN9 BER test for the TX operation with the PN9 sequence with the 6.52 GHz channel
- 6: TX_CHA PN23 BER test for the TX operation with the PN23 sequence with the 6.52 GHz channel
- 7: RX_CHA PN9 BER test for the RX operation with the PN9 sequence with the 6.52 GHz channel
- 8: RX_CHA PN23 BER test for the RX operation with the PN23 sequence with the 6.52 GHz channel
- 9: XTAL Test Crystal test to calibrate the crystal frequency
- A: TX_CHA TX test in the VRo mode with 1 ms intervals at the 6.52 GHz channel
- B: TX_CHB TX test in the VRo mode with 1 ms intervals at the 7.04 GHz channel
- C: TX_VRC TX test in the VRo mode with 1 ms intervals at the 7.56 GHz channel