13.3.4 DIAG_WDT_WindowedTimer
This API checks the WDT reset in window mode either the timer being cleared too early or too late. This test should not be called from main. The test will be executed before main is entered as long as diag_wdt_windowed_timer.h/.c is included in the compilation.
This diagnostics tests that window mode works by attempting to reset the WDT counter in the closed part of the WDT counter window. The correct response of the device should be to reset the device. The next step will test that WDT will issue a system reset in window mode if no WDR instruction is executed. If the device and WDT was reset correctly in each step of the test, then the diag_wdt_window_teststate is set to DIAG_WDT_WINDOW_FSM_OK and diag_windowed_wdt_status_t Enum is set to DIAG_WDT_WINDOW_PASS, otherwise the diag_wdt_window_teststate is set to DIAG_WDT_WINDOW_FSM_FAULT and diag_windowed_wdt_status_t Enum is set to DIAG_WDT_WINDOW_FAIL thereby indicating fault.
Error reporting:DIAG_WDT_WindowedTimer_GetStatus should be called from main to know the status of Windowed Timer WDT diagnosisvoid DIAG_WDT_WindowedTimer(
void
)
Returns
| void | See DIAG_WDT_WindowedTimer_GetStatus |