33.5.6 Low-pass Filter Mode
The Low-pass Filter mode (ADMD = 100
) acts similarly to the Average mode in how it handles samples (accumulates
samples until ADCNT value greater than or equal to ADRPT, then triggers threshold
comparison), but instead of a simple average, it performs a low-pass filter operation on
all of the samples, reducing the effect of high-frequency noise on the average, then
performs a threshold comparison on the results. (see Computation Operation for a more detailed description of the mathematical operation). In this mode, the ADCRS
bits determine the cutoff frequency of the low-pass filter (as demonstrated by Digital Filter/Average).