5 Appendix: Running the Tcl Script—Reference Design
(Ask a Question)Tcl scripts are provided in https://www.microchip.com/en-us/application-notes/an4684.
To run Tcl, perform the following steps:
- Launch the Libero® software.
- From the menu bar, click .
- In the downloaded directory
mpf_an4684_v20xxpx_df, locate and select thescript.tclfile. - To execute the selected Tcl script, click Run.
Upon successful execution, the Libero project is created within the top directory of
mpf_an4684_v20xxpx_df. You can verify the process by reviewing the log
file, see mpf_an4684_v20xxpx_df_log.
To understand the folder structure and details of the Tcl scripts and commands, see TCL_Scripts_readme.txt file and the Tcl Commands Reference Guide. For any queries about running the Tcl script, contact Technical Support.