5.3 Programming the PolarFire Device using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire Video kit with the .job file
using FlashPro Express. The .job file mpf_an4684_v20xxpx_jb
to test on PolarFire Video kit is provided in the Test Setup Prerequisites section.
To program the PolarFire device, perform the following steps:
- On the host PC, start the FlashPro Express software from its installation directory.
- To create a new job project on the Project menu, click New or New Job Project from FlashPro Express Job.
- In the New Job Project from FlashPro Express Job dialog box, perform the following steps:
- Programming job file: Click Browse and navigate to the location where the job file is located and select the file. The default location is mpf_an4686_v20xxpx_jb
- FlashPro Express job project location: Select Browse and navigate to the location where you want to save the project.
- Click OK. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears.
- Verify that a programmer number appears in the Programmer box. If it does not, verify the board connections and click Refresh/Rescan Programmers.
- To program the device, click RUN. When the device is programmed successfully, a RUN PASSED status is displayed.
- To close FlashPro Express, click .
- Close FlashPro Express or in the Project tab, click Exit.