8.1.3 FFD Project Configuration
Modify the following files to develop the Push Pull Star application.
Files to be modified to create demoapp_ffd project :
app.hdemo_app_ffd.happ.cdemo_app_ffd.cdemo_app_security.cusr_mac_callbacks.c
Note: In addition to this , pin settings and configuration settings for External Interrupt
Controller (EIC) must be done to configure User button as an interrupt to queue data on
the Co-ordinator.
The macros that are listed in the above files can be customized to modify the behavior of
the application. For instance, the macros found in demo_app_ffd.h can
be altered to modify the PAN ID and Short Address of the Co-ordinator.
demo_app_ffd.h