4 Getting Started with Software Development

This section gives a detailed information on the steps to install IDE, compiler, tool chain, wireless stacks and application examples on the PC. Prior to each release, the wireless stack and application examples are thoroughly tested against a snapshot of tool versions and other software dependencies. This guide provides information on setting up the development environment with all the required dependency versions and provide detailed steps to fulfill all the dependencies.

If the user is already familiar with Microchip Tools, then the following table summarizes the dependencies.

Tools and Harmony Component Versions

Tool Chain

Table 4-1. Tool Chain
IDE, Compiler and MCC PluginVersionLocation
MPLAB® X IDE6.25MPALB X IDE 6.25
XC32 compilerv4.60 or aboveMPLAB XC32 C/C++ Compiler
Microchip Code Configurator (MCC)5.6.2 or above See Installing the MPLAB® Code Configurator (MCC) Plugin from Related Links
Device Family Pack (PIC32CX-BZ3_DFP)1.3.216Microchip Packs Repository
CMSIS Packs6.2.0Navigate to Project Properties>Confg>Packs>CMSIS. For more details, see Opening , Building and Programming an Existing Application Example section of Running a Precompiled Application Example from Related Links.
Note: This table specifies the minimum required dependencies for the package versions.

Harmony Components

Use Content Manager (CM) to download the following Harmony components.

It will download the Harmony components to C:\Users\XXX\.mcc\harmony\content.

Table 4-2 4-4. Harmony Components
Harmony Components to be Cloned with MCC Content ManagerVersion
cspv3.22.7
corev3.15.5
bspv3.22.0
FreeRTOS-Kernelv11.1.0
CMSIS_55.9.0
wireless_blev1.5.0
wireless_pic32cxbz_wbzv1.6.0
wireless_system_pic32cxbz_wbzv1.8.1
wireless_threadv1.3.0
openthreadmchp_harmony_wireless_thread_v1.3.0
wireless_15_4_macv1.2.0
wireless_15_4_phyv1.4.0
Touchv3.18.1

For example, input “wireless_ble” in Content Manager and press Enter. Then choose the version specified in the above table. Finally, press “Apply” to download it. Please download all the required components specified in the above table.

The downloaded components will be under .mcc/harmony/content/. For example, the wireless_ble v1.5.0 will be in the following directory.

Application Example

Use Microchip Discover to download the following example code.

The application code can be downloaded to any folder and no requirement to be reside in C:\Users\XXX.mcc\harmony\content. Therefore, users can decide on their own folder and download the code. There are different categories of application code. This user guide only describes wireless_apps_pic32cxbz3_wbz35. Users can find the user guide of other application code when they click the link provided in the table.
Table 4-3. Application Example
NameVersionApplications
wireless_apps_pic32cxbz3_wbz35v1.2.0Wireless with below applications
core_apps_pic32cxbz3_wbz3(1)v3.2.0Peripheral driver
csp_apps_pic32cxbz3_wbz3(1)v3.2.0System middleware
Note:
  1. To migrate into latest environment, refer Upgrading MPLABX Projects to MCC (v5.6.2 or above) and Harmony Components.

Insert the above “Name” in the search field to find the example in Microchip Discover.

For more details, refer Download Application Example from Discover in Running a Precompiled Application Example from Related Links.

Another way is to download the application code directly from Microchip-MPLAB-Harmony Github. Insert the above “Name” in the repository field and download the example code.
Choose the version and the download method. As mentioned before, the application code can be downloaded to any folder.