1.1.1.1.1 DRV_AK4953_Deinitialize Function
void DRV_AK4953_Deinitialize( SYS_MODULE_OBJ object)
Summary
Deinitializes the specified instance of the AK4953 driver module.
Description
Deinitializes the specified instance of the AK4953 driver module, disabling its operation (and any hardware). Invalidates all the internal data.
Preconditions
Function DRV_AK4953_Initialize should have been called before calling this function.
Parameters
Parameters | Description |
---|---|
object | Driver object handle, returned from the DRV_AK4953_Initialize routine |
Returns
None.
Remarks
Once the Initialize operation has been called, the De-initialize operation must be called before the Initialize operation can be called again. This routine will NEVER block waiting for hardware.
Example
SYS_MODULE_OBJ object; _\/\/ Returned from DRV_AK4953_Initialize_ SYS_STATUS status; DRV_AK4953_Deinitialize(object); status = DRV_AK4953_Status(object); if (SYS_MODULE_DEINITIALIZED != status) { _\/\/ Check again later if you need to know_ _\/\/ when the driver is deinitialized._ }
C
void DRV_AK4953_Deinitialize(SYS_MODULE_OBJ object);