1.1.3.6.2 DRV_GENERICCODEC_MicGainSet Function
void DRV_GENERICCODEC_MicGainSet(DRV_HANDLE handle, uint8_t gain)
Summary
This function sets the microphone gain for the Generic Codec CODEC.
Description
This functions sets the microphone gain value from 0-31
Preconditions
The DRV_GENERICCODEC_Initialize routine must have been called for the specified Generic Codec driver instance.
DRV_GENERICCODEC_Open must have been called to obtain a valid opened device handle.
Parameters
Parameters | Description |
---|---|
handle | A valid open-instance handle, returned from the driver's open routine |
gain | Gain value, in range 0-31 |
Returns
None.
Remarks
None.
Example
_// myAppObj is an application specific object._
MY_APP_OBJ myAppObj;
_// myGENERICCODECHandle is the handle returned // by the DRV_GENERICCODEC_Open function._
DRV_GENERICCODEC_MicGainSet(myGENERICCODECHandle, 15); _//GENERICCODEC mic gain set to 15_
C
void DRV_GENERICCODEC_MicGainSet(DRV_HANDLE handle, uint8_t gain);