1.1.5.4.5 DRV_I2S_ProgrammableClockSet Function

bool DRV_I2S_ProgrammableClockSet(DRV_HANDLE handle, uint8_t pClkNum, uint8_t div2);

Summary

Set the Programmable Clock

Description

Set the Programmable Clock ignoring glitch control

Preconditions

None.

Returns

True - if the function was successful

False - if a timeout occurred (no transitions seen)

Remarks

None.

Example

_// myI2SHandle is the handle returned_ _// by the DRV_I2S_Open function._

DRV_I2S_ProgrammableClockSet(myI2SHandle, 2, 7);

C

bool DRV_I2S_ProgrammableClockSet(DRV_HANDLE handle, uint8_t pClkNum, uint8_t div2);