1.4.2.75 DSP_VectorLog10 Function
Computes the Log10(x), of the first N elements of inVector, and stores the result in outVector.
Description
void DSP_VectorLog10(_Q3_12 *outVector, _Q16 *inVector, int N);
Computes the Log10(x) value, on the first N elements of inVector. The output is stored to outVector. Input vector is _Q16 format, which is 32-bit data with 15 bits for the integer and 16 bits for the fractional portion. The output vector is reduced resolution Q3.12 format, which is a 16-bit integer format with 12 bits representing the fractional resolution. If values exceed maximum or minimum they will saturate to the maximum or zero respectively.
Preconditions
The pointers outdata and indata must be aligned on 4-byte boundaries. This function uses the Log10 function from the LibQ library. That library must be compiled as part of the project.
Parameters
outdata pointer to destination array of elements (_Q16)
indata pointer to source array of elements (_Q3_12)
N number of samples (int)
Returns
None.
Remarks
This function uses the Microchip PIC32MZ LibQ library to function. The user must include that library and header file into the design in order to operate this function. For more information on the Log10 function see the LibQ documentation for _LIBQ_Q3_12_log10_Q16. A negative number input will return a saturated negative value (0x8000).
Example
int logNum = 4; _Q16 inLogVal[8] = {0x40000000, 0xffff0000,0x00020000,0x00100000,0x00038000, 0x00400000,0xfffe0000,0x00058000}; _// 16384.0, -1.0, 2.0, 16.0, 3.5, 64.0, -2.0, 5.5_ _Q3_12 outLogVal[8] = {0}; DSP_VectorLog10(outLogVal, inLogVal, logNum); _// outLogVal = 0x436E, 0x8000, 0x04D1, 0x1344, 0, 0, 0, 0_ _// 4.2144, sat negative, 0.3010, 1.2041, 0, 0, 0, 0_
C
void DSP_VectorLog10 (_Q3_12 * outVector , _Q16 * inVector , int N );