1.1.5.2.1 DRV_I2S_Open Function

DRV_HANDLE DRV_I2S_Open

(

const SYS_MODULE_INDEX index, const DRV_IO_INTENT ioIntent

)

Summary

Opens the specified I2S driver instance and returns a handle to it.

Description

This routine opens the specified I2S driver instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the driver. The ioIntent parameter defines how the client interacts with this driver instance.

Specifying a DRV_IO_INTENT_EXCLUSIVE will cause the driver to provide exclusive access to this client. The driver cannot be opened by any other client.

Preconditions

Function DRV_I2S_Initialize must have been called before calling this function.

Parameters

ParametersDescription
indexIdentifier for the object instance to be opened
intentZero or more of the values from the enumeration DRV_IO_INTENT "ORed" together to indicate the intended useof the driver. See function description for details.

Returns

If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).

If an error occurs, the return value is DRV_HANDLE_INVALID. Error can occur

  • if the number of client objects allocated via DRV_I2S_CLIENTS_NUMBER is insufficient.

  • if the client is trying to open the driver but driver has been opened exclusively by another client.

  • if the driver peripheral instance being opened is not initialized or is invalid.

  • if the client is trying to open the driver exclusively, but has already been opened in a non exclusive mode by another client.

  • if the driver is not ready to be opened, typically when the initialize routine has not completed execution.

Remarks

The handle returned is valid until the DRV_I2S_Close routine is called. This routine will NEVER block waiting for hardware. If the requested intent flags are not supported, the routine will return DRV_HANDLE_INVALID. This function is thread safe in a RTOS application.

Example

DRV_HANDLE handle; handle = DRV_I2S_Open(DRV_I2S_INDEX_0, DRV_IO_INTENT_EXCLUSIVE); if (DRV_HANDLE_INVALID == handle) {

_// Unable to open the driver_

_// May be the driver is not initialized or the initialization_ _// is not complete._

}

C

DRV_HANDLE DRV_I2S_Open(const SYS_MODULE_INDEX index, const DRV_IO_INTENT ioIntent);