1.1.4.7.2 DRV_WM8904_VersionGet Function
uint32_t DRV_WM8904_VersionGet( void )
Summary
This function returns the version of WM8904 driver
Description
The version number returned from the DRV_WM8904_VersionGet function is an unsigned integer in the following decimal format. * 10000 + * 100 + Where the numbers are represented in decimal and the meaning is the same as above. Note that there is no numerical representation of release type.
Preconditions
None.
Returns
returns the version of WM8904 driver.
Remarks
None.
Example 1
For version "0.03a", return: 0 * 10000 + 3 * 100 + 0 For version "1.00", return: 1 * 100000 + 0 * 100 + 0
Example 2
uint32_t WM8904version; WM8904version = DRV_WM8904_VersionGet();
C
uint32_t DRV_WM8904_VersionGet();