1.1.4.5.1 DRV_WM8904_BufferAddRead Function
void DRV_WM8904_BufferAddRead ( const DRV_HANDLE handle, DRV_WM8904_BUFFER_HANDLE *bufferHandle, void *buffer, size_t size )
Summary
Schedule a non-blocking driver read operation.
Description
This function schedules a non-blocking read operation. The function returns with a valid buffer handle in the bufferHandle argument if the read request was scheduled successfully. The function adds the request to the hardware instance receive queue and returns immediately. While the request is in the queue, the application buffer is owned by the driver and should not be modified. The function returns DRV_WM8904_BUFFER_HANDLE_INVALID
if a buffer could not be allocated to the request
if the input buffer pointer is NULL
if the buffer size is 0.
if the queue is full or the queue depth is insufficient
If the requesting client registered an event callback with the driver, the driver will issue a DRV_WM8904_BUFFER_EVENT_COMPLETE event if the buffer was processed successfully of DRV_WM8904_BUFFER_EVENT_ERROR event if the buffer was not processed successfully.
Preconditions
The DRV_WM8904_Initialize routine must have been called for the specified WM8904 device instance and the DRV_WM8904_Status must have returned SYS_STATUS_READY.
DRV_WM8904_Open must have been called to obtain a valid opened device handle. DRV_IO_INTENT_READ must have been specified in the DRV_WM8904_Open call.
Parameters
Parameters | Description |
---|---|
handle | Handle of the WM8904 instance as return by the DRV_WM8904_Open function. |
buffer | Data to be transmitted. |
size | Buffer size in bytes. |
bufferHandle | Pointer to an argument that will contain the return buffer handle. |
Returns
The bufferHandle parameter will contain the return buffer handle. This will be DRV_WM8904_BUFFER_HANDLE_INVALID if the function was not successful.
Remarks
This function is thread safe in a RTOS application. It can be called from within the WM8904 Driver Buffer Event Handler that is registered by this client. It should not be called in the event handler associated with another WM8904 driver instance. It should not otherwise be called directly in an ISR.
C
void DRV_WM8904_BufferAddRead(const DRV_HANDLE handle, DRV_WM8904_BUFFER_HANDLE * bufferHandle, void * buffer, size_t size);