1.1.1.1.5 DRV_AK4953_Status Function
SYS_STATUS DRV_AK4953_Status(SYS_MODULE_OBJ object)Summary
Gets the current status of the AK4953 driver module.
Description
This routine provides the current status of the AK4953 driver module.
Preconditions
Function DRV_AK4953_Initialize should have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| object | Driver object handle, returned from the DRV_AK4953_Initialize routine |
Returns
SYS_STATUS_DEINITIALIZED - Indicates that the driver has been deinitialized
SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed
SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed
SYS_STATUS_ERROR - Indicates that the specified module is in an error state
Remarks
A driver can opened only when its status is SYS_STATUS_READY.
Example
SYS_MODULE_OBJ object; _\/\/ Returned from DRV_AK4953_Initialize_
SYS_STATUS AK4953Status;
AK4953Status = DRV_AK4953_Status(object); if (SYS_STATUS_READY == AK4953Status) {
_\/\/ This means the driver can be opened using the_ _\/\/ DRV_AK4953_Open() function._
}C
SYS_STATUS DRV_AK4953_Status(SYS_MODULE_OBJ object);