1.1.4.7.4 DRV_WM8904_LRCLK_Sync Function
uint32_t DRV_WM8904_LRCLK_Sync (const DRV_HANDLE handle);
Summary
Synchronize to the start of the I2S LRCLK (left/right clock) signal
Description
This function waits until low-to high transition of the I2S LRCLK (left/right clock) signal (high-low if Left-Justified format, this is determined by the PLIB). In the case where this signal is generated from a codec or other external source, this allows the caller to synchronize calls to the DMA with the LRCLK signal so the left/right channel association is valid.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
Returns
True - if the function was successful
False - if a timeout occurred (no transitions seen)
Remarks
None.
Example
_// myWM8904Handle is the handle returned_ _// by the DRV_WM8904_Open function._ DRV_WM8904_LRCLK_Sync(myWM8904Handle);
C
bool DRV_WM8904_LRCLK_Sync(const DRV_HANDLE handle);